Does any test eMMC 5.0 on i.mx53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does any test eMMC 5.0 on i.mx53

966 Views
MaxChou
Contributor III


Dear  ALL

Does anyone  test eMMC 5.0 chip boot from i.mx53 ?

thank you very much!!

Max.

3 Replies

677 Views
woodyshao
Contributor I

Maybe It can. The default firmware mmc.c in MX53 is different from that in iMX6.

0 Kudos

677 Views
igorpadykov
NXP Employee
NXP Employee

Hi Max

I am afraid it can not, since

i.MX53 ROM checks eMMC ()MC_SPEC_VER_4_X  version before proceed.

In software you can try method below

i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

677 Views
MaxChou
Contributor III

Hi  Igor

thanks for your reply,

i am also afraid mx53 rom code can't support eMMC 5.0,

just wants to confirm it.

I had tested eMMC 4.51 is no problem,

Max

0 Kudos