Does T-topology achieve 4GByte DDR3 configuration with i.MX6Q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does T-topology achieve 4GByte DDR3 configuration with i.MX6Q?

跳至解决方案
1,421 次查看
nahoko
Contributor I

Hello,

I am trying to implement 4GB DDR3 for i.MX6Q. Depending on the Hardware Development Guide, T topology design is limited to 4 DDR chips.

> -your design is limited to 4 DDR chips.

> -DDR3, 2GByte using latest memories (4GBytes coming)  (<- Is this really "Byte" ? or "2Gbit / chip"?)

Does it mean that only Fly-by topology can achieve 4GByte configuration?

AW designer says that it's hard to achieve the layout requirement of Fly-by topology with 8 of DDR3 chips and they want to use T-topology.

Thank you.

标签 (1)
0 项奖励
回复
1 解答
869 次查看
Yuri
NXP Employee
NXP Employee

  According to the i.MX6 design Checklist, it is suggested to use "T" topology

when the number of DDR3 chips are not more than four.  Otherwise "Fly-by"

Topology is recommended, since it allows to decrease timing / trace length

requirements because of additional calibration procedures.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
870 次查看
Yuri
NXP Employee
NXP Employee

  According to the i.MX6 design Checklist, it is suggested to use "T" topology

when the number of DDR3 chips are not more than four.  Otherwise "Fly-by"

Topology is recommended, since it allows to decrease timing / trace length

requirements because of additional calibration procedures.

0 项奖励
回复
869 次查看
nahoko
Contributor I

Thank you very much for your reply.

0 项奖励
回复