Does T-topology achieve 4GByte DDR3 configuration with i.MX6Q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does T-topology achieve 4GByte DDR3 configuration with i.MX6Q?

Jump to solution
1,322 Views
nahoko
Contributor I

Hello,

I am trying to implement 4GB DDR3 for i.MX6Q. Depending on the Hardware Development Guide, T topology design is limited to 4 DDR chips.

> -your design is limited to 4 DDR chips.

> -DDR3, 2GByte using latest memories (4GBytes coming)  (<- Is this really "Byte" ? or "2Gbit / chip"?)

Does it mean that only Fly-by topology can achieve 4GByte configuration?

AW designer says that it's hard to achieve the layout requirement of Fly-by topology with 8 of DDR3 chips and they want to use T-topology.

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
770 Views
Yuri
NXP Employee
NXP Employee

  According to the i.MX6 design Checklist, it is suggested to use "T" topology

when the number of DDR3 chips are not more than four.  Otherwise "Fly-by"

Topology is recommended, since it allows to decrease timing / trace length

requirements because of additional calibration procedures.

View solution in original post

0 Kudos
Reply
2 Replies
771 Views
Yuri
NXP Employee
NXP Employee

  According to the i.MX6 design Checklist, it is suggested to use "T" topology

when the number of DDR3 chips are not more than four.  Otherwise "Fly-by"

Topology is recommended, since it allows to decrease timing / trace length

requirements because of additional calibration procedures.

0 Kudos
Reply
770 Views
nahoko
Contributor I

Thank you very much for your reply.

0 Kudos
Reply