Does MCIMX6SX-SDB have emmc interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MCIMX6SX-SDB have emmc interface?

Jump to solution
2,325 Views
JHY
Contributor IV

SPF-27962.pdf describes that MCIMX6SX-SDB has only foot print for eMMC interface.

Is it possble to test eMMC using MCIMX6SX-SDB?

e.jpg

Labels (1)
Tags (1)
1 Solution
2,100 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

eMMC can be used after soldering on this foot print, for tests

one can follow sect.4.4.1.2 Using eMMC attached Linux Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,101 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

eMMC can be used after soldering on this foot print, for tests

one can follow sect.4.4.1.2 Using eMMC attached Linux Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------