Does L3.14.52_1.1.0-ga BSP support PF3000 for i.MX6SL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does L3.14.52_1.1.0-ga BSP support PF3000 for i.MX6SL?

Jump to solution
617 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about pf3000.

According to AN5113 sect. 3, we have to contact a local NXP representative for BSP patch for the PF3000 with i.MX6SL.

Is this same at latest linux BSP (L3.14.52_1.1.0-ga)?

Or the latest BSP have supported PF3000 for i.MX6SL already?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
408 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems not, as there is no dts file for PF3000 with i.MX6SL (like imx6sl-evk-pf3000.dts )

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts?h=imx_3.14.52_1.1...

Best regards

igor
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
409 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems not, as there is no dts file for PF3000 with i.MX6SL (like imx6sl-evk-pf3000.dts )

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts?h=imx_3.14.52_1.1...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos