Dear community.
We are investigating 1bit ECC nand which support ONFI.
- Spansion, S34ML04G100TFI000
As far as we checked, it was recognised correctly both uboot and kernel with below information.
ECC 1bit, oob 64 bytes, Size 512M bytes
And it also passed erase/write/compare test over 1000 times.
Could you double check whether IMX6SoloX support this memory ?
FYI, u-boot and kernel version are like below.
- U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0
- Linux version 3.14.52-1.1.0
BR
Jace
Hi Jace
yes i.MX6SoloX supports 1bit ECC NAND.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------