Do you support DPRAM in IMX6DualLite?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you support DPRAM in IMX6DualLite?

1,802件の閲覧回数
mingyue-liu
Contributor I

Hi, we want to use the HMS product anybus in the I.MX6 DualLite SOC.

From anybus datasheet, we saw that the anybus have a DPRAM to exchange data with imx6, and we should use parallel addr/data bus from anybus's DPRAM to connect to the imx6.

So, do the imx6 support DPRAM? if yes, how to support it?

the anybus's datasheet is at the attachment.

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,693件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can reffer to the thread https://community.nxp.com/message/854790 

Have a nice day

Rita

0 件の賞賛
返信

1,693件の閲覧回数
mingyue-liu
Contributor I

Hello Rita,

Thankyou for reply.

Do you mean that we can use EIM to connect to the DPRAM which is in anybus?

The DPRAM which is in anybus is 4Kbytes, 12 address lines, 8 data lines, with OE, RW, CE control lines.

the EIM only support 8/16/32 address lines, so which lines could we choose?

and there no CE line in the EIM

0 件の賞賛
返信