Do you have some benchmark data of i.MX6DL GPU with OpenCL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you have some benchmark data of i.MX6DL GPU with OpenCL?

ソリューションへジャンプ
2,102件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Do you have some benchmark data of i.MX6DQ GPU when it is used for GPGPU with OpenCL?

Any benchmark soft is ok, but it is better if the data includes the CPU (Cortex-A9 in i.MX6DQ) performance also to compare CPU vs GPU performance.

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid there is no such official data.

In general one can look at next helpful links

EEMBC -- The Embedded Microprocessor Benchmark Consortium

LMbench Benchmarks on i.MX

Benchmarking the GPU bandwidth capability based on OpenCL memory copy operation | allontutorials

The computing power of the Vivante's GC2000 GPU in i.mx6q (more)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,269件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am afraid there is no such official data.

In general one can look at next helpful links

EEMBC -- The Embedded Microprocessor Benchmark Consortium

LMbench Benchmarks on i.MX

Benchmarking the GPU bandwidth capability based on OpenCL memory copy operation | allontutorials

The computing power of the Vivante's GC2000 GPU in i.mx6q (more)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信