Do you have i.MX6DQ input load capacitance data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you have i.MX6DQ input load capacitance data?

Jump to solution
1,162 Views
satoshishimoda
Senior Contributor I

Hi communty

Do you have a data about "input" load capacitance of i.MX6DQ CSI0_DAT pins?

Especially, we want to know about CSI0_DAT4, CSI0_DAT5, and CSI0_DAT7 pins.

Best Regards,

Satoshi Shimoda

Labels (2)
0 Kudos
Reply
1 Solution
1,091 Views
Yuri
NXP Employee
NXP Employee

  To know capacity values of i.MX6 signals - please use corresponding IBIS model.

(assuming standard input model scheme, specified in IBIS )

  Also let me remind, if R_pin, L_pin, and C_pin parameters (FOR THAT PIN ONLY !)

are not declared, this means the default package values (R_pkg, L_pkg, C_pkg,

specified under [Package]) should be used.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,092 Views
Yuri
NXP Employee
NXP Employee

  To know capacity values of i.MX6 signals - please use corresponding IBIS model.

(assuming standard input model scheme, specified in IBIS )

  Also let me remind, if R_pin, L_pin, and C_pin parameters (FOR THAT PIN ONLY !)

are not declared, this means the default package values (R_pkg, L_pkg, C_pkg,

specified under [Package]) should be used.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply