Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do the timers in i.MX6ULL can support quadrature (incremental) encoder input ?

1,789 Views
jimmyli
Contributor IV

Hi,

     We are evaluting the i.MX6ULL for our project.

     In the project, we need to encode one magnetic encoder quadrature input (A/B), and one signal output.

     We find i.MX6ULL has not QDC, so we consider that if the timer in i.mx6ull can support this function?

     Hope you can help to check with us.

     Thanks very much.

Labels (1)
0 Kudos
Reply
4 Replies

1,738 Views
jimmychan
NXP TechSupport
NXP TechSupport

There is no QDC in i.MX6ULL. So the feature is not supported.

0 Kudos
Reply

1,736 Views
jimmyli
Contributor IV

Hi Jimmychan,

      Get it. Thanks.

      Yes, i.MX6ULL hasn't QDC, so I conside that whether the quadrature encoder inputs can be captured by GPT capture function, but I still can't be sured about it.

      Do you have some tips for this ?

      Thanks.

jimmyli_0-1712481873545.png

----i.MX6ULL GPT capture function

 

0 Kudos
Reply

1,717 Views
jimmychan
NXP TechSupport
NXP TechSupport

I searched around internal database and cannot find any example code about this.

0 Kudos
Reply

1,690 Views
jimmyli
Contributor IV

Hi Jimmychan,

       Get it.

       Thanks very much.

0 Kudos
Reply