Do the plugin of imxvideoconvert_ipu support convert YUY2 to RGB24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do the plugin of imxvideoconvert_ipu support convert YUY2 to RGB24

2,158 Views
adamzhu
Contributor I

I convert color space from YUY2 to RGB24 by hardware path. But it cannot be  included YUY2 format in caps of imxvideoconvert_ipu . However, in spec file of imx6q , said it can support any one of color formats defined in MPEG-4 standard.

Labels (3)
0 Kudos
Reply
2 Replies

1,427 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may look at  section 7.3.15 (Video conversion) of "i.MX_Linux_User's_Guide.pdf"

in recent Linux BSP doc package.

"Use gst-inspect-1.0 to get each convertor's capability and supported input and output formats."

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617...

In particular :

root@imx6qdlsolo:~# gst-inspect-1.0 imxvideoconvert_ipu

Factory Details:

  Rank                     primary + 1 (257)

  Long-name                IMX ipu Video Converter

  Klass                    Filter/Converter/Video

  Description              Video CSC/Resize/Rotate/Deinterlace.

  Author                   Multimedia Team <shmmmw@freescale.com>

Plugin Details:

  Name                     imxvideoconvert.imx

  Description              IMX Video Convert Plugins

  Filename                 /usr/lib/gstreamer-1.0/libgstimxvideoconvert.so

  Version                  4.0.9

  License                  LGPL

  Source module            imx-gst1.0-plugin

  Binary package           Freescle Gstreamer Multimedia Plugins

  Origin URL               http://www.freescale.com

GObject

+----GInitiallyUnowned

       +----GstObject

             +----GstElement

                   +----GstBaseTransform

                         +----GstVideoFilter

                               +----imxvideoconvert_ipu

Pad Templates:

  SRC template: 'src'

    Availability: Always

    Capabilities:

      video/x-raw

                 format: { I420, NV12, YV12, UYVY, RGB16, RGBx, Y42B, Y444, v308, BGR, RGB, BGRx, BGRA, RGBA, ABGR }

      video/x-raw(memory:SystemMemory, meta:GstVideoOverlayComposition)

                 format: { I420, NV12, YV12, UYVY, RGB16, RGBx, Y42B, Y444, v308, BGR, RGB, BGRx, BGRA, RGBA, ABGR }

  SINK template: 'sink'

    Availability: Always

    Capabilities:

      video/x-raw

                 format: { I420, NV12, YV12, UYVY, RGB16, RGBx, Y42B, Y444, v308, BGR, RGB, BGRx, BGRA, RGBA, ABGR }

      video/x-raw(memory:SystemMemory, meta:GstVideoOverlayComposition)

                 format: { I420, NV12, YV12, UYVY, RGB16, RGBx, Y42B, Y444, v308, BGR, RGB, BGRx, BGRA, RGBA, ABGR }

Element Flags:

  no flags set

Element Implementation:

  Has change_state() function: gst_element_change_state_func

Element has no clocking capabilities.

Element has no URI handling capabilities.

Pads:

  SINK: 'sink'

    Pad Template: 'sink'

  SRC: 'src'

    Pad Template: 'src'

Element Properties:

  name                : The name of the object

                        flags: readable, writable

                        String. Default: "imxvideoconvert_ipu0"

  parent              : The parent of the object

                        flags: readable, writable

                        Object of type "GstObject"

  qos                 : Handle Quality-of-Service events

                        flags: readable, writable

                        Boolean. Default: true

  rotation            : Rotation that shall be applied to output frames

                        flags: readable, writable

                        Enum "ImxVideoConvertRotationMode" Default: 0, "none"

                           (0): none             - No rotation

                           (1): rotate-90        - Rotate 90 degrees

                           (2): rotate-180       - Rotate 180 degrees

                           (3): rotate-270       - Rotate 270 degrees

                           (4): horizontal-flip  - Flip horizontally

                           (5): vertical-flip    - Flip vertically

  deinterlace         : Deinterlacing mode to be used for incoming frames (ignored if frames are not interlaced)

                        flags: readable, writable

                        Enum "ImxVideoConvertDeinterlaceMode" Default: 0, "none"

                           (0): none             - No deinterlace

                           (1): low-motion       - low-motion deinterlace

                           (2): mid-motion       - midium-motion deinterlace

                           (3): high-motion      - high-motion deinterlace

  composition-meta-enable: Enable overlay composition meta processing

                        flags: readable, writable

                        Boolean. Default: false

  in-place            : Handle composition meta in place in pass through mode, video overlay composition will blended onto input buffer

                        flags: readable, writable

                        Boolean. Default: false

root@imx6qdlsolo:~#

Regards,

Yuri.

0 Kudos
Reply

1,427 Views
art
NXP Employee
NXP Employee

Most likely, your version of imxvideoconvert_ipu does not support the YUY2 format. Type 'gst-inspect-1.0 imxvideoconvert_ipu' for the list of supported formats.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply