Do all USDHC ports support SDR104?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do all USDHC ports support SDR104?

跳至解决方案
1,970 次查看
hiroshisekoguch
Contributor I

Hello,

There is the sentence "For UHSI cards, clock speed fuses can be set to SDR50 or SDR104 on USDHC3 and USDHC4 ports" in IMXDQRM .

Does this mean USDHC1 and USDHC2 don't support SDR104?

Best Regards

0 项奖励
回复
1 解答
1,516 次查看
Yuri
NXP Employee
NXP Employee

Looks as inaccuracy in the RM.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,516 次查看
Yuri
NXP Employee
NXP Employee

   According to the Datasheet :

"All four ports support:

• 1-bit or 4-bit transfer mode specifications for SD and SDIO cards up to

UHS-I SDR104 mode (104 MB/s max) ...".  

   As for boot mode, please refer to Table 5-7 (SD/eSD Boot Fusemap) and

Table 5-8 (MMC/eMMC Boot Fusemap) of the i.MX6 DQ Reference Manual.

Regards,

Yuri.

0 项奖励
回复
1,516 次查看
hiroshisekoguch
Contributor I

Hi Yuri,

Thank you for your reply.

I see all four ports support UHS-I SDR104 mode, but what does the sentence below mean?

"For UHSI cards, clock speed fuse can be set to SDR50 or SDR104 on USDHC3 and USDHC4 ports" in chapter 8.5.3.3 'SD,eSD and SDXC'

Regards,

Hiroshi Sekoguchi


0 项奖励
回复
1,517 次查看
Yuri
NXP Employee
NXP Employee

Looks as inaccuracy in the RM.

Regards,

Yuri.

0 项奖励
回复