Do all USDHC ports support SDR104?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do all USDHC ports support SDR104?

ソリューションへジャンプ
1,967件の閲覧回数
hiroshisekoguch
Contributor I

Hello,

There is the sentence "For UHSI cards, clock speed fuses can be set to SDR50 or SDR104 on USDHC3 and USDHC4 ports" in IMXDQRM .

Does this mean USDHC1 and USDHC2 don't support SDR104?

Best Regards

0 件の賞賛
返信
1 解決策
1,513件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks as inaccuracy in the RM.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,513件の閲覧回数
Yuri
NXP Employee
NXP Employee

   According to the Datasheet :

"All four ports support:

• 1-bit or 4-bit transfer mode specifications for SD and SDIO cards up to

UHS-I SDR104 mode (104 MB/s max) ...".  

   As for boot mode, please refer to Table 5-7 (SD/eSD Boot Fusemap) and

Table 5-8 (MMC/eMMC Boot Fusemap) of the i.MX6 DQ Reference Manual.

Regards,

Yuri.

0 件の賞賛
返信
1,513件の閲覧回数
hiroshisekoguch
Contributor I

Hi Yuri,

Thank you for your reply.

I see all four ports support UHS-I SDR104 mode, but what does the sentence below mean?

"For UHSI cards, clock speed fuse can be set to SDR50 or SDR104 on USDHC3 and USDHC4 ports" in chapter 8.5.3.3 'SD,eSD and SDXC'

Regards,

Hiroshi Sekoguchi


0 件の賞賛
返信
1,514件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks as inaccuracy in the RM.

Regards,

Yuri.

0 件の賞賛
返信