Do SPI transfers through DMA block CPU ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do SPI transfers through DMA block CPU ?

Jump to solution
3,171 Views
bastien_cornut
Contributor I

Hello,

I am currently working with imx SPI driver on an imx6. I am using a kernel based on the 3.10 branch of linux-fslc.

I am not used to DMA transfer, but what I understand about DMA is that they should let the CPU do others tasks when a transfer through DMA is in progress.

But I have the feeling that when the DMA transfer is initialized and then triggered, the CPU is waiting actively for DMA transfer to finish.

In the following code, I see a call to wait_for_timeout_completion which is a not interruptible function. Can you confirm me that this means that when my CPU perform a SPI transfer it is blocked waiting the end of the DMA transfer ?

static int spi_imx_dma_transfer(struct spi_imx_data *spi_imx,
struct spi_transfer *transfer)
{
struct dma_async_tx_descriptor *desc_tx = NULL, *desc_rx = NULL;
int ret;
int left = 0;
struct spi_master *master = spi_imx->bitbang.master;
struct sg_table *tx = &transfer->tx_sg, *rx = &transfer->rx_sg;
if (tx) {
desc_tx = dmaengine_prep_slave_sg(master->dma_tx,
tx->sgl, tx->nents, DMA_TO_DEVICE,
DMA_PREP_INTERRUPT | DMA_CTRL_ACK);
if (!desc_tx)
goto no_dma;
desc_tx->callback = spi_imx_dma_tx_callback;
desc_tx->callback_param = (void *)spi_imx;
dmaengine_submit(desc_tx);
}
if (rx) {
struct scatterlist *sgl_last = &rx->sgl[rx->nents - 1];
unsigned int orig_length = sgl_last->length;
int wml_mask = ~(spi_imx->rx_wml - 1);
/*
* Adjust the transfer lenth of the last scattlist if there are
* some tail data, use PIO read to get the tail data since DMA
* sometimes miss the last tail interrupt.
*/
left = transfer->len % spi_imx->rx_wml;
if (left)
sgl_last->length = orig_length & wml_mask;
desc_rx = dmaengine_prep_slave_sg(master->dma_rx,
rx->sgl, rx->nents, DMA_FROM_DEVICE,
DMA_PREP_INTERRUPT | DMA_CTRL_ACK);
if (!desc_rx)
goto no_dma;
desc_rx->callback = spi_imx_dma_rx_callback;
desc_rx->callback_param = (void *)spi_imx;
dmaengine_submit(desc_rx);
}
reinit_completion(&spi_imx->dma_rx_completion);
reinit_completion(&spi_imx->dma_tx_completion);
/* Trigger the cspi module. */
spi_imx->dma_finished = 0;
spi_imx->devtype_data->trigger(spi_imx);
dma_async_issue_pending(master->dma_tx);
dma_async_issue_pending(master->dma_rx);
/* Wait SDMA to finish the data transfer.*/
ret = wait_for_completion_timeout(&spi_imx->dma_tx_completion,
IMX_DMA_TIMEOUT(transfer->len));
if (!ret) {
pr_warn("%s %s: I/O Error in DMA TX:%x\n",
dev_driver_string(&master->dev),
dev_name(&master->dev), transfer->len);
dmaengine_terminate_all(master->dma_tx);
} else {
ret = wait_for_completion_timeout(&spi_imx->dma_rx_completion,
IMX_DMA_TIMEOUT(transfer->len));
if (!ret) {
pr_warn("%s %s: I/O Error in DMA RX:%x\n",
dev_driver_string(&master->dev),
dev_name(&master->dev), transfer->len);
spi_imx->devtype_data->reset(spi_imx);
dmaengine_terminate_all(master->dma_rx);
} else if (left) {
/* read the tail data by PIO */
void *tmpbuf = transfer->rx_buf + transfer->len - left;
while (readl(spi_imx->base + MX51_ECSPI_STAT) & 0x8) {
*(char *)tmpbuf =
readl(spi_imx->base + MXC_CSPIRXDATA);
tmpbuf++;
}
}
}
spi_imx->dma_finished = 1;
spi_imx->devtype_data->trigger(spi_imx);
if (!ret)
ret = -ETIMEDOUT;
else if (ret > 0)
ret = transfer->len;
return ret;
no_dma:
pr_warn_once("%s %s: DMA not available, falling back to PIO\n",
dev_driver_string(&master->dev),
dev_name(&master->dev));
return -EAGAIN;

}

0 Kudos
Reply
1 Solution
2,783 Views
igorpadykov
NXP Employee
NXP Employee

Hi

sorry you are right, it waits for sdma completion, however seems it does not prevent

other threads to be executed.

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,780 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bastien

nxp sdma driver do not use this function, one can check sect.4.1.3 Source Code Structure

attached Linux Manual and sources on

linux-2.6-imx.git - Freescale i.MX Linux Tree 

linux-2.6-imx.git - Freescale i.MX Linux Tree 

linux-fslc is community branch and supported by community, it may be posted on

meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale

difference between Yocto Community BSP and Freescale BSP Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,780 Views
bastien_cornut
Contributor I

Hi,

Actually, this function "wait_for_completion_timeout" is called in the imx spi driver: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.10.17... (see function spi_imx_dma_transfer, line 958)

My question was to know if the CPU is actually polling the end of dma transfer or do I misunderstand the workflow of a spi dma transfer ?

Regards,

Bastien

0 Kudos
Reply
2,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi

sorry you are right, it waits for sdma completion, however seems it does not prevent

other threads to be executed.

Best regards
igor

0 Kudos
Reply