Do I need to pull up PMIC_ON_REQ externally?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do I need to pull up PMIC_ON_REQ externally?

Jump to solution
960 Views
yan_ding
Contributor I

Hi,

I have a quick question on the port "PMIC_ON_REQ". According to page 113 of "IMX7ULPCEC", the state is Output/High. So, is this a DC output port to the PMIC? To de-assert this signal, I can pull it down through a switch or IC.

Do I need to pull up this signal externally? 

Thanks,

Yan

Labels (1)
Tags (2)
0 Kudos
1 Solution
874 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yan

no need to pull up this signal externally.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
875 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yan

no need to pull up this signal externally.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
874 Views
yan_ding
Contributor I

Thank you igor.

0 Kudos