Displayed images of videos using OpenCV are strange

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Displayed images of videos using OpenCV are strange

6,956 Views
taiki_kasamatsu
Contributor I

I am now using the IMX8QXP-CPU Board (rev. c0) to load videos with OpenCV and simply display them.


When I load the video with cv2.VideoCapture, the size of the image is loaded correctly, but when I display it with imshow, the display is strange as shown in the attached image.

here is my code (I didn't quite understand how to make it a code block, sorry.)

import cv2

#load movie
cap = cv2.VideoCapture('RiverDance.mp4')

while True :
    ret, img = cap.read()
    height, width, channels = img.shape[:3]
    print("width: " + str(width))
    print("height: " + str(height))

    cv2.imshow('Video', img)
    k = cv2.waitKey(1)
    if k==27: # Esc key to stop
        break

I also performed image processing methods such as importing still images, displaying the imported images, exporting, grayscale conversion, Gaussian smoothing, and binarization.
It worked without any problems.

---Types of videos I've tried :

mp4, width:1280, height: 720, 59.94 fps
mp4, width:640, height: 360, 29.97 fps

mp4, width:480, height: 272, 24.0 fps

The same result was obtained for avi, mov, and mkv.

--- about OS info :

ID="fsl-imx-xwayland"
NAME="NXP i.MX Release Distro"
VERSION="4.14-sumo (sumo)"
VERSION_ID="4.14-sumo"
PRETTY_NAME="NXP i.MX Release Distro 4.14-sumo (sumo)"

--- about Python & OpenCV :

Python 3.5.5 (didn't use any virtualenv include pyenv)
[GCC 7.3.0] on linux
>>> import cv2
>>> cv2.__version__
'4.0.1'

Can anyone tell me what causes this and what the solution is?
I'm sorry to bother you, but I would appreciate your help.

thanks in advance.

0 Kudos
Reply
10 Replies

6,902 Views
Anonymous
Deactivated User

ha taiki,

try this:

import cv2
import numpy as np

#load movie
cap = cv2.VideoCapture(0)

while True :
ret, img = cap.read()
height, width, channels = img.shape[:3]
print("width: " + str(width))
print("height: " + str(height))

cv2.imshow('Video', img)
k = cv2.waitKey(1)
if k==27: # Esc key to stop
break

thanks

Kalaimani Arumugam

0 Kudos
Reply

6,893 Views
taiki_kasamatsu
Contributor I

Thank you for your answer!


From the looks of it, the python source you gave me is to imshow the input image from the camera, right?In this case, there is no problem when the input is from the camera, but when the input is from a video file such as mp4, a strange image like the one attached is displayed.

0 Kudos
Reply

6,880 Views
Anonymous
Deactivated User

hai taiki,

   I am generating the issue here for fix. i need some check operation done there

1.Is it work with normal web camera application.

cap = cv2.VideoCapture(0)  

 2. Also check the image operation in imshow.

cap = cv2.imread('''Image Location''')

Thanks

kalaimani Arumugam 

0 Kudos
Reply

6,874 Views
taiki_kasamatsu
Contributor I

hi kalaimani,

1. Yes, This works with no problems. I can show the image from some cameras properly.

cap = cv2.VideoCapture(0)  

 

2. This is also working and I can get it's sizes and show properly

cap = cv2.imread('''Image Location''')

 

Thank you.

0 Kudos
Reply

6,870 Views
Anonymous
Deactivated User

 hai taiki, 

   Till now i am not getting this issue. Try to Uninstall and install the "openCV" 

 

Thanks

Kalaimani Arumugam

 

 

0 Kudos
Reply

6,860 Views
taiki_kasamatsu
Contributor I

kalaimani

Thank you for trying.
I'll try some things here as well.

Thanks!

0 Kudos
Reply

6,944 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello taiki,

 

You should use the Linux 5.4.70_2.3.0​ for python 4. I just the same procedure on my pc with the same result, but If i change for python 4 it pass, so please try it.

 

Regards

 

0 Kudos
Reply

6,908 Views
taiki_kasamatsu
Contributor I

Thank you for your answer.
After that I did some research and it seems that python4 doesn't exist yet, which version of python4 are you referring to?

0 Kudos
Reply

6,842 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Sorry there is no python 4, the latest version is python 3.9.

 

Regards

 

0 Kudos
Reply

6,821 Views
takayuki_ishii
Contributor V

Hello @Bio_TICFSL 

I have same problem on i.MX8QXP MEK + Linux BSP L5.4.70_2.3.0.

So please teach me which method do you use to install python3.9 to Linux BSP L5.4.70_2.3.0?

 1) Add package of python3.9 to local.conf and bitbake

 2) Download python3.9 source code and configure/make/make install it.

 3) Some other method like "pip update"

 

I look forward to hearing from you.

 

Best regards,

Ishii.

0 Kudos
Reply