Display not working: Android IMX8 Quad Max

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display not working: Android IMX8 Quad Max

3,018 Views
dgohlya
Contributor I

./uuu_imx_android_flash.sh -f imx8qm -a -e -u trusty

Used the above command to flash android to HW. On rebooting was able to see the display, android was succeessfully installed.

 

On removing the cable and rebooting again, the Display was gone.

How can I bring back the display?

Tags (1)
0 Kudos
Reply
5 Replies

3,003 Views
dgohlya
Contributor I

Android 10.

I removed the power cable and rebooted. I also tried removing the HDMI display and trying again. That did not work too.

0 Kudos
Reply

2,988 Views
joanxie
NXP TechSupport
NXP TechSupport

android 10 what?android 10.0.0_2.5.0?

do you mean you remove the power cable then insert the power cable back, the board couldn't boot up again? anything output from the uart port?

0 Kudos
Reply

2,956 Views
dgohlya
Contributor I

I have attached the minicom logs.

11.0.0_1.0.0_DEMO_8Q and  Q10.0.0_2.6.0_DEMO_8Q were the images I tried withWe also looked at android logcat and we see this:

Like I said, we did see the display once and cannot see it anymore.

Another piece of information is, we see the below in adb logcat logs


E display : updateScreen invalid drmfd

0 Kudos
Reply

2,816 Views
joanxie
NXP TechSupport
NXP TechSupport

I have tested android 11.0.0_2.0.0, I couldn't reproduce this issue

1) connect the hdmi then boot up, then disconnect the cable then connect back, the hdmi display come back

2) connect the hdmi and boot up, then disconnect the cable of hdmi, then reboot up the board and connect the cable back, the hdmi display shows the logo successfully

0 Kudos
Reply

3,004 Views
joanxie
NXP TechSupport
NXP TechSupport

On removing the cable and rebooting again, the Display was gone

>what cable do you mean? did you remove the cable between board and display?

do you mean you remove the cable between board and display, then connect the cable and reboot again?

and what android version do you use?

 

0 Kudos
Reply