Display enabling for IMX6 Ull evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display enabling for IMX6 Ull evk board

381 Views
athul_am
Contributor II

Hi,

I have acquired a NXP imx6ull evk board.I would like to use a ubuntu image on the board and show the ubuntu UI on a Screen.I would like to know 2 things :

1.if a specific image is to be used , i would like to know which one.

2.Can i connect the OTG port to a Hdmi connector and show on a screen,if not how to connect a display.

thanks,

Athul

Labels (1)
0 Kudos
Reply
3 Replies

309 Views
athul_am
Contributor II

Hi @Alejandro_Salas ,

i would like to know one more thing, this is the board i am going to use:https://www.sunfounder.com/products/10inch-touchscreen-for-raspberrypi

Can you please let me know if this is compatible with the board?

thanks and Regards,

Athul

0 Kudos
Reply

309 Views
athul_am
Contributor II

Hi @Alejandro_Salas ,

sorry for the late Response and thank you for your response.

I need to show a vehicle dashboard setup in the display so was thinking of using python for the same, will it be possible with linux bsp?

Thanks and Regards,

athul

0 Kudos
Reply

359 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @athul_am 

 

Unfortunately, Ubuntu is not supported in the i.MX6ULL , but you can download our Linux BSP from the official web page.

You can connect an LCD display through  the LCD connector:

Alejandro_Salas_0-1714053684697.png

 

Best regards.

 

Salas.

0 Kudos
Reply