Display board interface in i.MX 6SX Sabre

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display board interface in i.MX 6SX Sabre

616 Views
kanimozhi_t
Contributor V

Hi,

We're planning to use i.MX 6SX Sabre board for our development and confused on the display interface.

Currently we have,

  1. NXP iMX6UL Display LCD8000-43T - LCD expansion port connector
  2. NXP iMX8M MIPI-DSI 1080p OLED Display - MIPI-DSI Display mini-SAS connector

So, the current questions are,

  1. Can we use any of the above mentioned with i.MX 6SX Sabre board?
  2. Is the "LCD expansion connector (parallel, 24-bit)" on i.MX 6SX compatible with LCD8000-43T?
Labels (1)
0 Kudos
Reply
1 Reply

553 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the two display you can not directly use.

For the i.MX 6SX Sabre board default support display are the followings.

https://www.nxp.com/part/MCIMX-LVDS1#/

https://www.nxp.com/part/MCIMX28LCD#/

  • LVDS connector
    • Pairs with MCIMX-LVDS1 LCD display board
  • LCD expansion connector (parallel, 24-bit)
    • Pairs with MCIMXHDMICARD adapter board