Dear all,
I successfully tested meta-imx-fde-demo - imx_sec_apps - i.MX Security Application Examples full disk encryption patch on kernel 4.14 applying patch by hand
I want to integrate it in kernel 4.19 and after applying those patches, also by hand, everything compiles well and key blob is properly generated
However, device mapper launches following error when calling dmsetup
caam_jr 30901000.jr0: caam algorithms can't process tagged key
device-mapper: table: 253:0: crypt: Error decoding and setting key
device-mapper: ioctl: error adding target to table
Development board is MCIMX7SABRE (device status is OPEN)
Linux kernel tested are linux-imx_4.14.78_1.0.0_ga and linux-imx_4.19.35_1.1.0 from linux-imx - i.MX Linux kernel CodeAurora NXP repository
Reference documentation AN12714 i.MX Encrypted Storage Using CAAM Secure Keys
Can any one give me some help ?
Thanks in advance
Jorge R
已解决! 转到解答。
Hi all,
After been in contact with my local NXP FAE, I would like to share the solution to my problem
This functionality is already available on the L.5.4.47-2.2.0 and the latest L.5.4.70-2.3.0 Linux BSPs
Tested on L.5.4.70-2.3.0 and works as expected !
Hi
I follow AN12714 Rev. 0 — 25 February 2020,
I also tested meta-imx-fde-demo - imx_sec_apps - i.MX Security Application Examples full disk encryption patch on kernel 4.14.98 applying patch by hand,but the file in ./mnt/encrypted unencrypted, I do not know why and how to solve. my platform is imx6ul
thanks
Hi all,
After been in contact with my local NXP FAE, I would like to share the solution to my problem
This functionality is already available on the L.5.4.47-2.2.0 and the latest L.5.4.70-2.3.0 Linux BSPs
Tested on L.5.4.70-2.3.0 and works as expected !
After been in contact with my local NXP FAE, I would like to share the requested functionality is now available in latest Yocto BSP L5.4.47_2.2.0
Not tested yet, but promising it is already official and in NXP BSP mainline !
Hi Yuri,
Thanks for your message
This is my first NXP information request and after revising the information given at NXP technical portal it is not clear to me how to proceed
Do you want me to contact ProSupport ?
Does that require a paid contract between my company and NXP ?
May I have to wait for kernel 5.7 availability and stop trying any other kernel higher than 4.14 ?
I also tested applying demo-caam-blobs 0001-black-key-blob-after-4.14ga-changes-and-license-iden.patch, which is quite similar to kernel 4.14 patch, but with no success on 4.19 disk encryption !
Regards
Yocto Linux BSP used is L4.19.35_1.1.0 downloaded from https://source.codeaurora.org/external/imx/imx-manifest (the latest available when I started working with MCIMX7SABRE last December)