Disk Partition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Disk Partition

1,118 次查看
1990rahulreddy
Contributor IV

I am following, "i.MX 6Dual/6Quad SABRE-SD Linux User's Guide, Rev. L3.0.35_4.1.0, 09/2013", In this they have given 16384 [starting at offset sector #16384, But It shows mi following error. Any Help ...My target is run OpenCv on this Board & Linaro ALIP is available for this. or Is there any way to install openCV & Ubuntu..in L3.14.28_1.0.0.

.sdcard    require no partition,But, I have to Install Ubuntu, so I am following this Document.

标签 (2)
0 项奖励
回复
1 回复

795 次查看
b36401
NXP Employee
NXP Employee

It seems the log was actually not attached to the message.

So I can provide only common recomendation.

Please refer 4.3.3 Partitioning the SD/MMC card chapter of i.MX Linux User's Guide.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复