Hi all,
I am using sabre automotive board with i.mx6q. I built yocto linux into it.
I need to disable X11 and wayland/weston. Is there a way to disable them without modifying another distro.
If no, how can I do it with modifying distro and how can I show new distro to MFG tool?
yocto has different image you can choose, if you don't need x11, you can choose "core-image-minimal", which is A small image that only allows a device to boot. or choose "core-image-base", which is A console-only image that fully supports the target device hardware.