Hi NXP Team,
We are using i.MX8MQ processor in our project and we have a requirement of performing the following things:
I wanted to know if the above-mentioned things are possible on i.MX8MQ processor? If yes, can you please help me out with the steps for the same?
Thanks in advance.
Regards
Meetali Patel
Solved! Go to Solution.
Hi Meetali
for 1,2 one can refer to SDP_DISABLE fuse in Table 6-40. Boot Fusemap, also
additional info was sent via mail
i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual
for 3. one can look at
https://stackoverflow.com/questions/57671588/disabling-uart-debug-serial-port-on-linux
Best regards
igor
Hi Meetali
for 1,2 one can refer to SDP_DISABLE fuse in Table 6-40. Boot Fusemap, also
additional info was sent via mail
i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual
for 3. one can look at
https://stackoverflow.com/questions/57671588/disabling-uart-debug-serial-port-on-linux
Best regards
igor
Hi @igorpadykov ,
I tried fusing the SJC_DISABLE register but still, I am able to detect my device using the JTAG interface. Is this an expected behavior? I used the following command at u-boot to fuse this register:
$ fuse prog 1 3 0x200000
Also, I have not yet fused SDP_DISABLE register but I am not able to detect the device from the UUU tool.
Can you please share some more detailed information about the SDP_DISABLE and SJC_DISABLE fuse registers?
Thanks & Regards
Meetali Patel
Hi @igorpadykov,
I am now able to disable serial download and JTAG using the steps mentioned.
Thanks for the support.
Regards
Meetali Patel