Disable data lines in suspend mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable data lines in suspend mode

1,212件の閲覧回数
HelbertPaulino
Contributor I

Hello everyone,

I'm trying to compile a Yocto image that must disable data lines for PCIe, USB1, USB2, LVDS, and ETH1 (RGMII) when entering suspend mode and restoring the original state after waking up. Basically, for other devices, I'm changing the pinctrl to use another configuration of pin to decrease the power consumption, but these peripherals I'm not finding a way to disable them.


My findings suggest creating a driver to write some registers when entering suspend mode, but I don't know if it'll solve the problem. I tried to find in the bindings some configurations in the device tree but with not much success (only some possibilities to interact with regulators, but nothing so much different from implementing a driver).

Please, can someone give me tips or a direction about a good way to disable these peripherals? I'm a beginner doing this.

Thanks very much for the support.

0 件の賞賛
返信
3 返答(返信)

1,193件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HelbertPaulino,

I hope you are doing well.

"disable these peripherals?"
->Please refer to the below link, It has detailed information regarding how to disable any peripheral on the system using the device tree status property.
https://www.variscite.com/blog/disabling-unused-drivers-and-peripherals-in-linux/

It will be helpful.

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信

1,187件の閲覧回数
HelbertPaulino
Contributor I

Hello @Sanket_Parekh,

Thanks very much for replying to me. My case is a bit different from the case covered in the link, because, basically, I need to use these devices in my system, thus I can't disable them in the Device Tree.

For some peripherals, I'll be using another pinctrl to control the IOMUX pins, put as output low, however, for the mentioned devices I'm not finding a way to change the data lines in suspend mode.

Am I able to set the status for "disable" in the user space before entering in suspend mode?

Thanks very much for helping me.

Regards





0 件の賞賛
返信

1,165件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HelbertPaulino,

I hope you are doing well.

Please refer to the drivers that are mentioned in the below link.
https://github.com/nxp-imx/linux-imx?search=1

The suspend and resume function is already provided in the Linux bsp 6.1 version.

I hope this will help you.

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信