Disable Debug Logs in imx8mp EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable Debug Logs in imx8mp EVK

1,523 Views
its_abhi07
Contributor I

Hi Team,

We are using NXP IMX8MP EVK for our project. We have seen that there is only 3 Build mode available for the same [eng, user, userdebug]. So what we want is to disable the debug logs [especially the boot logs] and needed adb. But by default configurations, these two wont be possible in one go. So we tried to change the value of ro.debuggable=1 to 0 [File -> out/target/product/evk_8mm/system/build.prop]. But we are still facing the same.

Could anyone help for the same? 
Requirement : Adb enabled and Boot logs disabled [which is equivalent to a performance build] .
Platform : NXP IMX8M PLUS

Thanks,
Abhiram

0 Kudos
Reply
2 Replies

1,513 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @its_abhi07 

Please change ro.debuggable  value in default.prop

0 Kudos
Reply

1,511 Views
its_abhi07
Contributor I

Hi Qmiller,

Thanks for the response, we changed the value of ro.debuggable to zero for disabling the debug logs. 
File = out/target/product/evk_8mp/recovery/root/default.prop

But found that still the kernel logs are there. Also this file is generated only after one initial build [default.prop]. So we changed the value after the initial build and builded again. Thats how we checked. 

Is this the correct way or could you please correct if I our steps are wrong?.

Thanks,
Abhiram

0 Kudos
Reply