Disable AGL Reference UI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable AGL Reference UI

1,132件の閲覧回数
donjacobvellathottam
Contributor III

I have built an AGL image using yocto. But I can't disable the reference ui (home screen of agl).

I tried building other images than agl-demo-platform, like agl-image-weston but then there isn't anything in the display at all.

I've also tried to edit the config files and set the default compositor to weston still it doesn't work.

 

Eighter it shows the refrence ui or it is complete blank(with a single cursor blinking)

How can I Disable the reference ui and replace agl-compositor with weston/wayland.

0 件の賞賛
返信
2 返答(返信)

1,090件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

If you are using Yocto from NXP, the start of AGL/weston is controlled by systemctl, you should find that service and disable it. 

0 件の賞賛
返信

1,032件の閲覧回数
donjacobvellathottam
Contributor III
sorry but i wasn't able to find weston services in systemctl
0 件の賞賛
返信