Disable AGL Reference UI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Disable AGL Reference UI

1,141 次查看
donjacobvellathottam
Contributor III

I have built an AGL image using yocto. But I can't disable the reference ui (home screen of agl).

I tried building other images than agl-demo-platform, like agl-image-weston but then there isn't anything in the display at all.

I've also tried to edit the config files and set the default compositor to weston still it doesn't work.

 

Eighter it shows the refrence ui or it is complete blank(with a single cursor blinking)

How can I Disable the reference ui and replace agl-compositor with weston/wayland.

0 项奖励
回复
2 回复数

1,099 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

If you are using Yocto from NXP, the start of AGL/weston is controlled by systemctl, you should find that service and disable it. 

0 项奖励
回复

1,041 次查看
donjacobvellathottam
Contributor III
sorry but i wasn't able to find weston services in systemctl
0 项奖励
回复