Directly exchange packets from ethernet ports in i.MX 6SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Directly exchange packets from ethernet ports in i.MX 6SoloX

620 Views
MelissaArosemen
NXP Employee
NXP Employee

As there’s no internal switch on the Ethernet controllers to directly pass packets from one Gb port to another, is there a way to do this without a switch? If not do you have any idea what overhead will be needed to pass them back and forth?

Tags (1)
0 Kudos
Reply
1 Reply

527 Views
b36401
NXP Employee
NXP Employee

He have no ready solution of a switch based on i.MX processor.

I only know that there are some solutions for router. For example OpenWrt does support i.MX6.

Here I found a common discussion regarding to Linux based switch:

https://www.reddit.com/r/linux/comments/1f2ss7/

However please note that i.MX series are more multimedia than networking processors.

For networking purposes we can recomend some another processor.

Something like this:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=P4080

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply