Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply

435 Views
AndreyMyachkov
Contributor I

Have a nice day!

During a detailed study of the demo board electrical scheme for the IMX8MMini, I noticed that the output of the microprocessor B25 (RTC_XTALO) is directly connected to the 0V8 power supply.

Based on the above, please respond:

1) is this a mistake ?

2) is it allowed to connect the output of the RTC_XTALO microprocessor directly to the 0V8 power supply via a 0Ohm resistor ?

I think it's best to connect this pin B25 (RTC_XTALO) to the 0V8 power supply via a 1kOhm resistor !

What do you think about it ?

Looking forward to hearing from you.

Thanks a lot,

Best regards,

Andrey Myachkov

0 Kudos
Reply
2 Replies

402 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello.

It is correct, 0Ohm resistor is used for testing purposes on the EVK.

According to the datasheet, RTC_XTALO should be directly connected to VDD_SNVS_0P8, then 1k ohm is not necessary.

Regards. 

0 Kudos
Reply

383 Views
AndreyMyachkov
Contributor I

Hi!

Thanks a lot for your reply.

Best regards.

Andrew

0 Kudos
Reply