Digital silicon Microphone with I2S interface connect to I.MX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Digital silicon Microphone with I2S interface connect to I.MX6ULL

ソリューションへジャンプ
1,806件の閲覧回数
KuiLu
Contributor I

I  have 2 I2S digital microphone with I2S interface,

KuiLu_0-1644288819405.png

 

The connection with iMX6ULL will be:

I2S_CLK -> CSI_DATA05 -> SAI1_TX_BCLK;

I2S_WS -> CSI_DATA04 -> SAI1_TX_SYNC;

I2S_DATA -> CSI_DATA06 -> SAI1_RX_DATA;

Will this correct?

If this pads config to ESAI, will be worked also?

0 件の賞賛
返信
1 解決策
1,732件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,733件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

0 件の賞賛
返信
1,723件の閲覧回数
KuiLu
Contributor I

Artur, thanks. Lu Kui

0 件の賞賛
返信