Different contents on multiple display imx6 android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Different contents on multiple display imx6 android

2,699 次查看
kirangv
Contributor III

Hello,

I want to display different contents on dual display connected to imx6 running android.

Currently i am able to mirror the contents on both HDMI and LVDS , but help me on displaying different contents on both displays ?  

Platform : iMX6Q SABRE-AI

OS : Android Marshmallow

Application QT : 5.7

Display : HDMI and LVDS

0 项奖励
回复
5 回复数

2,133 次查看
gary_bisson
Senior Contributor III

Hi,

You need to leverage the Presentation API:

Presentation | Android Developers 

Not sure how well it is integrated into Qt though.

Here is an example where we start two different application, one on each display:

Android Lollipop dual display/app demo on i.MX6 - Boundary Devices 

Note that it works on Marshmallow too.

Regards,

Gary

2,131 次查看
kirangv
Contributor III

Thank you for the reply. We will check this approach.

Also looking for any other better approach for QT application. 

0 项奖励
回复

2,131 次查看
joanxie
NXP TechSupport
NXP TechSupport

as I known, you can install the HDMIshow.apk, which supports this. you can try it.

0 项奖励
回复

2,131 次查看
joshua_hong
Contributor III

Hi Joan Xie,

I would like to try the HDMIshow.apk too. can you provide the resource for me to download this apk?

thank you and have a nice week ahead.

0 项奖励
回复

2,131 次查看
kirangv
Contributor III

Hi Joan,

I could not get HDMIshow.apk or the source related to it , can you provide me a path from i can download this.

Thanks,

Kiran

0 项奖励
回复