Different between kernel 3.0.xx vs 3.10.xx vs 3.14.xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Different between kernel 3.0.xx vs 3.10.xx vs 3.14.xx

1,381 Views
zctee
Contributor III

Hi all,

I notice that in the Freescale page for i.mx6, there are 3 version of linux, which are 3.0.101, 3.10.53 and 3.14.28.

i.MX 6 Series Software and Development Tool R|Freescale

May i know what is the different between these 3 version of linux BSP?

Thank you.

Regards,

ZC

Labels (2)
Tags (2)
0 Kudos
3 Replies

675 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZC

difference is decribed in Release Notes document included in

Doc bundle for each package (in particular pay attention to sect.2.x New features)

L3.0.35_4.1.0_LINUX_DOCS

L3.14.28_1.0.0_LINUX_DOCS

L3.10.53_1.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

675 Views
zctee
Contributor III

Hi Igor,

It seems like the 3.0.xx is for Debian, while 3.10.xx and 3.14.xx is for yocto. Am i correct to say that?

Thank you.

Regards,

ZC

0 Kudos

675 Views
zctee
Contributor III

Hi Igor,

Is there any doc package for the 3.0.101? It seems that i only can find latest doc till 3.0.35 in below page:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Regards,

ZC

0 Kudos