Different POR behavior between MCIMX6Q-SDB and MCIMX6DL-SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Different POR behavior between MCIMX6Q-SDB and MCIMX6DL-SDP

955 Views
torus1000
Contributor V


Hi,

I compared two reference boards then found a difference.

In case of POR (JTAG_nSRST: pin15) asserted, MCIMX6DL-SDP rebooted but MCIMX6Q-SDB freezed.

I used same Linux versions for both of them.

Why POR caused such different results?

Can anyone explain me?

Labels (1)
Tags (2)
0 Kudos
5 Replies

712 Views
torus1000
Contributor V

What's the status now?

Any updates you may have would be greatly appreciated.

jamesbone

0 Kudos

712 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Torus,

There are several versions of the SABRE-SDP and SABRE-SDB boards, can you please clarify, the versions of the boards that you are seeing with a different behavior? So we can review the schematics and provide the changes and this may show the different behaviors in the POR.

0 Kudos

712 Views
b50231katsuhiro
NXP Employee
NXP Employee

Hi jamesbone

Torus is DFAE in a region, so could you please follow-up this case?

0 Kudos

712 Views
torus1000
Contributor V

Hi jamesbone,

Any update? I just want to make sure...

Thanks.jamesbone

0 Kudos

712 Views
torus1000
Contributor V

jamesbone

Dear jamesbone,

Here are my board's revisions:

- MCIMX6Q-SDB         SCH-27516 REV C4

- MCIMX6DL-SDP         SCH-27417 REV C2

Please have a look. It seems same circuit around JTAG_nSRST.

Thanks.

0 Kudos