I have an MCIMX7D-SABRE RevB (SCH-28590 Rev B), but the only schematic that I can find is for Rev D(SCH-28590 Rev D). Are there any major differences between the two and is there a Rev B schematic available? I'm trying to get support for SDR104 SD Cards, but can't get it to work in 1.8V mode.
Hello,
NVCC_SD1 supply voltage is provided by the PMIC on the i.MX7 SABRE
design. This voltage is configured using SD_VSEL signal of the PMIC:
SD_VSEL is input from i.MX processor (GPIO1_IO08 on the SABRE) to select
VCC_SD regulator voltage. So, SD1 supply voltage is programmable.
IMX7 GPIO1_IO08 default state is GPIO port, input, pulled down, therefore
just after reset NVCC_SD1 is 3 V. Customers cannot change it for SD1 boot,
but can modify the voltage after boot in OS.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------