Difference between imx503, imx51 and imx53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between imx503, imx51 and imx53

1,291件の閲覧回数
saurabh206
Senior Contributor III

Hi Community,

I want to know what is a difference between imx503, imx51 and imx53?

Does Yocto BSP support available for above processor?

Thanks

Saurabh

ラベル(5)
0 件の賞賛
返信
1 返信

1,109件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

for differencies one can look at

AN4271 Architectural Differences Between i.MX51 and i.MX53

IMX50FS i.MX50 Family of Applications Processors - Fact Sheet

seems imx51 and imx53 are supported by community yocto,

though I am not sure about imx503.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------