Difference between MCIMX6 and PCIMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MCIMX6 and PCIMX6

Jump to solution
1,566 Views
danielbujak
Contributor III

I've been developing on the MX6UL EVK with the PCIMX6G2CVM05AA, but am now looking to port to a custom PCB with the MCIMX6G2AVM07AA part on it. Where can I find information on the differences between these parts that I need to be aware of for the port?

Labels (1)
0 Kudos
Reply
1 Solution
1,339 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,340 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

0 Kudos
Reply
836 Views
brian_21
Contributor I

For Special Qualification level, is the SC marked at the package body for this type of device?

0 Kudos
Reply