Device details are verified before Public key verification, What are device details?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device details are verified before Public key verification, What are device details?

404件の閲覧回数
jiteshka
Contributor I

In the attached image Secure boot design is mention. As per the image, Device details are also verified. Any idea what is verified. Is it related to CSF-related details Verifications or something else?

jiteshka_0-1631882856158.png

 

0 件の賞賛
1 返信

393件の閲覧回数
Yuri
NXP Employee
NXP Employee

@jiteshka 
Hello,

  Device details fuses are analyzed - as shown on the figure - during Device Details
verification. For example, i.MX8M supports HDMI, which requires signed HDMI
firmware loading, but i.MX8Mm does not have HDMI and HDMI firmware
is not needed.

Regards,
Yuri.

0 件の賞賛