Device Tree To Support DDC/CI For HDMI On i.MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Tree To Support DDC/CI For HDMI On i.MX8

949件の閲覧回数
kendalla59
Contributor I

I have a small embedded HDMI display, and I would like to add some monitor controls into the user interface. The display supports DDC/CI but my i.MX8 device tree does not expose the i2c lines for the HDMI port. I've searched through the linux-imx/arch/arm64/boot/dts/freescale files, and I can't find any examples of this.

Can somebody please help me to get access to the dedicated SDA/SCL for the HDMI interface?

 

0 件の賞賛
3 返答(返信)

692件の閲覧回数
darko31
Contributor II

Hi we've had a similar problem with wanting to send commands over the DDC lines.

Take a look at the cdns_hdmi_scdc_write function.

https://github.com/nxp-imx/linux-imx/blob/lf-5.15.y/drivers/gpu/drm/bridge/cadence/cdns-mhdp-hdmi.c#...

It is possible create a custom function similar to the cdns_hdmi_scdc. The data can be hardcoded in the driver and called from initialization or via sysfs interface.

Just make sure to have the 0 and 1 in the message in the same way as in the cdns_hdmi_scdc_write function otherwise the packet isn't sent properly. I believe it's some kind of message protocol to the mailbox register of the HDMI IP but I'm not entirely sure.

Best regards,

Darko

0 件の賞賛

941件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what imx8 processor do you use? imx8qm?

 

0 件の賞賛

935件の閲覧回数
kendalla59
Contributor I

I'm using the i.MX 8M, I believe. It's a BCM AR8MXMQ board.

https://www.bcmcom.com/bcm_product_AR8MXMQ.html

0 件の賞賛