Developer board i.MX6 to support three / 3 displays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Developer board i.MX6 to support three / 3 displays

1,074件の閲覧回数
mikaelarhelger
Contributor I

Our project requires a total of three displays:

  • 4:3 x 2
  • 16: 9 x 1

Where can we obtain a developer board capable of this and configured for this?

ラベル(3)
タグ(2)
1 返信

939件の閲覧回数
EricNelson
Senior Contributor II

Our Nitrogen6x, Nitrogen6_Max, and BD-SL-i.MX6 boards each support three displays, as shown in the video here:

     http://boundarydevices.com/timesys-2013-03-release/

The only displays we offer have 16:9 aspect ratios though. Those with 4:3 are generally harder to find.

If you contact us at mailto:info@boundarydevices.com with your specific needs, it's possible that we have support for displays that match your criteria (sizes, resolution, touch interfaces).