Designing a Linux board using MCIMX6Y1?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Designing a Linux board using MCIMX6Y1?

661 次查看
iohertz
Contributor II

I am going to design a Linux board using MCIMX6Y1 processor. I am looking for JTAG that can be used with MCIMX6Y1 and other tools (hardware and software) that will be required for designing and running my Linux board.

Below is the list of components that I think will be required for my board:

  1. FT234XD (USB-To-Uart Bridge)
  2. KSZ8081 (Ethernet Transceiver)
  3. MT41K512M16 (LvDDR3)
  4. JTAG
  5. MCIMX6Y1
  6. Voltage Regulators
  7. Connectors

I am planning to boot my board via external SD card and therefore, I have skipped emmc, qspi or any other flash in my board to reduce the board cost and save space. Is it possible to boot from external sd card without any on-board emmc or flash? Can someone help me getting cheap JTAG? I am comfortable with Linux and open source tools. Can someone suggest me things that I will require and I have missed it in my list? Any component? Does IMX6ULL has SWD interface?.  I will share my design soon with the community to review it.

Thanks

标签 (2)
0 项奖励
1 回复

451 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek

for jtag usage one can check below links

Bring up i.MX6 via JTAG 

AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK

https://www.nxp.com/docs/en/application-note/AN5229.pdf 

AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励