Design Files for i.MX8 plus CPU board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Design Files for i.MX8 plus CPU board

582件の閲覧回数
rjm
Contributor IV

Two DRC errors are present in this design (besides numerous yellow warnings).

I'm caring about this since I started to created a gerber file set as a first step towards production of this SOM.

It points out that there are two unnamed nets that - very apparently with intention - each connects two pins on the board. Just a connection present in the board but not in the design file (using OrCAD 17.4-2019-S027).

To be precise:

  • U1 B11 is connected to J3.42 (while both pins are defined as NC in the schematic).
  • U1 E12 is connected to J3.48 (while both pins are defined as NC in the schematic).

Of course I'd prefer to establish these connections in the schematic. But before doing so, any feedback is appreciated.

 

 

 

ラベル(1)
0 件の賞賛
0 返答(返信)