Design Files for i.MX8 plus CPU board

取消
显示结果 
搜索替代 
您的意思是: 

Design Files for i.MX8 plus CPU board

282 次查看
rjm
Contributor IV

Two DRC errors are present in this design (besides numerous yellow warnings).

I'm caring about this since I started to created a gerber file set as a first step towards production of this SOM.

It points out that there are two unnamed nets that - very apparently with intention - each connects two pins on the board. Just a connection present in the board but not in the design file (using OrCAD 17.4-2019-S027).

To be precise:

  • U1 B11 is connected to J3.42 (while both pins are defined as NC in the schematic).
  • U1 E12 is connected to J3.48 (while both pins are defined as NC in the schematic).

Of course I'd prefer to establish these connections in the schematic. But before doing so, any feedback is appreciated.

 

 

 

0 项奖励
0 回复数