Dear All,
Hello.
Refer to 67.2 External Signals in IMX6DQRM(Rev.2).
The uSDHC4 signals exist.
But, the refer to 67.2 External Signals in IMX6DQRM(Rev.3), the uSDHC4 signals wasn't seen.
Is this typo?
Best Regards,
Keita
Solved! Go to Solution.
OK !
Hello,
i.MX6 DQ supports uSDHC4 port; so, the section 67.2 in the RM, rev.2 is not full.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
>i.MX6 DQ supports uSDHC4 port; so, the section 67.2 in the RM, rev.2 is not full.
No.
RM rev.2 was descripted about uSDHC4.
In RM rev.3, the description was lost.
Best Regards,
Keita
Sorry, my misprint : the section 67.2 in the RM, rev.3 is not full.
Hi Yuri,
OK. I think so, too.
Thank you very much.
If NXP has the plan of document update, please fix the typo.
Best Regards,
Keita