Hello,
While transferring data from iMX6UL to slave device using SPI, we are getting unnecessary pause between two bytes.
We have used ecspi3 in DMA mode and clock speed is 10MHz.
If transfer time for one byte is 800ns then pause between two bytes is half of this time i.e 400ns. If we increase/decrease clock speed then pause time is changing accordingly but half of the single byte transfer time.
Please see attached image.
How to reduce/remove this unnecessary delay between two bytes, please guide.
Thanks.