Decoding of h.264 content with the VPU requires more free framebuffers than indicated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Decoding of h.264 content with the VPU requires more free framebuffers than indicated

981 Views
dv1
Contributor III

Hello,

I observed something peculiar when working with the VPU decoder. The imx-vpu API informs me about how many framebuffers I need to prepare and register. According to the VPU API manual PDF, the minFrameBufferCount value in the DecInitialInfo indicate the minimum number of framebuffers required for decoding. So, using this minimum number should in theory be enough. Except, it isn't.

With some h.264 streams that use the h.264 high profile, I observed that this minimum is not enough. When retrieving information about the output picture by calling vpu_DecGetOutputInfo(), sometimes the indexFrameDisplay value of the DecOutputInfo struct contains the value -3. The VPU docs say about value -3 : "There is temporarily no display output even without any action by the host application. Usually, this value occurs when an IDR picture is received for H.264 display-reordering mode." Until now, I was working around this by allocating 6 extra framebuffers in addition to the number specified by minFrameBufferCount. With this, I never get -3.


Now, my question is: when I receive the index -3 , should I consider the frame dropped? Or just delayed? The text I quoted above indicates the latter, but I'd like some confirmation for this.

Labels (3)
0 Kudos
2 Replies

642 Views
gusarambula
NXP TechSupport
NXP TechSupport

The -3 should occur because there is no display output but should not drop the frame, only re-order it, if it makes sense.

Are you playing the video straight or skipping/rewinding? H.264 encoding configuration may change the ability to perform these actions with or without temporary distortion.

642 Views
dv1
Contributor III

Just straight playback. I have observed that the -3 value in indexFrameDisplay occurs in groups, followed by equally large groups of negative values in indexFrameDecoded. I am investigating this. Perhaps I can introduce an internal queue to queue up encoded frames. My findings will go to the libimxvpuapi library.

0 Kudos