Debug serial port on SABRE outputs rubbish

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug serial port on SABRE outputs rubbish

ソリューションへジャンプ
1,525件の閲覧回数
emil
Contributor III

I've just copied the images to the eMMC with the MFGTool using this option in the cfg.ini-file:

 

board=SabreSD

name=i.MX6DL-SABRESD-eMMC

Description:Download the u-boot, kernel and Linux rootfs to the eMMC

 

I have a usb cable conected to the USB to UART port and I can see things happening on the terminal. All of a sudden when booting up linux i start getting rubbish on the serial port. It seems like the bootup routine is doing something with the serial port. Also, I would like to know how to configure the boot environment variables so that I can get the video output on the touchscreen (which comes with the SABRE Smart Devices kit).

 

I'll attach the log from the serial output.

 

Thanks.

 

Original Attachment has been moved to: putty2013-03-19-104503.log.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,273件の閲覧回数
emil
Contributor III

For some strange reason it worked when I did the following:

Dual Display on IMX6Q in Android

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,274件の閲覧回数
emil
Contributor III

For some strange reason it worked when I did the following:

Dual Display on IMX6Q in Android

0 件の賞賛
返信