Debug serial port on SABRE outputs rubbish

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug serial port on SABRE outputs rubbish

Jump to solution
870 Views
emil
Contributor III

I've just copied the images to the eMMC with the MFGTool using this option in the cfg.ini-file:

 

board=SabreSD

name=i.MX6DL-SABRESD-eMMC

Description:Download the u-boot, kernel and Linux rootfs to the eMMC

 

I have a usb cable conected to the USB to UART port and I can see things happening on the terminal. All of a sudden when booting up linux i start getting rubbish on the serial port. It seems like the bootup routine is doing something with the serial port. Also, I would like to know how to configure the boot environment variables so that I can get the video output on the touchscreen (which comes with the SABRE Smart Devices kit).

 

I'll attach the log from the serial output.

 

Thanks.

 

Original Attachment has been moved to: putty2013-03-19-104503.log.zip

Labels (1)
0 Kudos
1 Solution
618 Views
emil
Contributor III

For some strange reason it worked when I did the following:

Dual Display on IMX6Q in Android

View solution in original post

0 Kudos
1 Reply
619 Views
emil
Contributor III

For some strange reason it worked when I did the following:

Dual Display on IMX6Q in Android

0 Kudos