Debix model B with Raspberry pi HQ camera (imx477)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debix model B with Raspberry pi HQ camera (imx477)

3,142 次查看
noklm
Contributor II

Hello everyone,

I recently bought the Debix model B based on IMX8M plus processor. The idea is to benchmark my computer vision application that is actually running on a Raspberry pi 4 with the HQ camera.

I want to keep my camera setup (HQ) because I need to change lenses (debix cameras cannot).

If I'm not wrong debix board seems to have all the necessary interface (CSI) and ISP to operate the Rpi HQ camera based on the imx477 sensor.

Have you some ressources (tutorial, drivers ...) to use this camera with the Debix ?

Thank you in advance

Regards

0 项奖励
回复
5 回复数

3,097 次查看
khang_letruong
Senior Contributor III

Hi @noklm ,

 

You will need to re-bitbake a custom image for that board using its u-boot and kernel here : https://github.com/debix-tech

The following document will guide you to develop an ISP based camera driver of iMX8MP :  https://www.nxp.com/docs/en/application-note/AN13713.pdf

Reference examples :

IMX219 :

- Doc : https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true

- Code : https://github.com/nxp-imx-support/imx8mp-imx219-sensor-enablement

IMX477 : https://community.nxp.com/t5/i-MX-Processors/Porting-IMX477-for-IMX8MP-Isp/m-p/1648414

 

 

 

 

 

0 项奖励
回复

3,104 次查看
noklm
Contributor II

Thank you for your reply you can have all detailed about the debix board here.

So maybe the only things I need to find is the device tree file et drivers then ? If someone have these I'm interrested

0 项奖励
回复

3,084 次查看
joanxie
NXP TechSupport
NXP TechSupport

your board should support imx477, not only dts file, you also need change isp and vvcam driver in your bsp, for more detailed information and demo code based on nxp bsp, you can refer to the links Khang shows

0 项奖励
回复

3,112 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you have more detailed information about Debix board? I can confirm that imx8mp can support imx477

0 项奖励
回复

3,012 次查看
noklm
Contributor II

Hello,

Thank you all for your replies.

I found a good discussion on the debix community on discord about camera with the Debix.

Kieran Bingham from libcamera is actually working on porting libcamera framework on debix based imx8mp. A demonstration was showcased. He shared the custom kernel with libcamera patches here:

https://gitlab.com/ideasonboard/nxp/linux

To use Mipi camera with the debix board you must have the debix IO board which is a shame.

Unfortunately I had no time to test it for now.

Regards