Hello everyone,
I have been stuck for days. I couldn't install debian packages using apt-get.
Even I added the apt-get command in the linux image, I couldn't install any of the packages.
I want to install scipy using pip and failed because there are some libraries package that should be installed like
libatlas-base-dev and gfortran.
Could anyone help ?
And if there is a complete debian image for the evk ?
Thank you in advance.
Best regards,
Hi Chayma
unfortunately nxp does not officially support debian, one can look at third party:
https://boundarydevices.com/wiki/debian-for-nitrogen8/
or Build Ubuntu For i.MX8 Series Platform
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your answer. I will look for the links you provided me.