Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

2,594 Views
charleshuang
Senior Contributor II

Hi NXP,

We are following the NXP Release Debian 2024/12/30 version as per the official documentation:

https://docs.nxp.com/bundle/UG10155/page/topics/building_an_image_in_flexbuild.html

We followed the standard procedure described in the "Most used examples with automated build" section and run the command:

blb -m imx8mpevk

We understand that this process may involve building a Debian Docker image with ML features.

Could you confirm whether it is possible to successfully compile the Docker image using this method?
If not, could you provide the correct SOP (Standard Operating Procedure) for building it?

We have strictly followed NXP's official SOP, but we are encountering issues.
Please let us know the correct steps to complete the build successfully.

Thanks,

 

 

build_fail.jpg

0 Kudos
Reply
6 Replies

2,578 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,559 Views
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

In the thread, you say : "Please use Ubunut22.04 as host environment."

So, do you mean we shouldn't use the Docker environment?

Please provide the correct the SOP.  Thanks.

0 Kudos
Reply

2,553 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If you need ML feature, you need use docker under Ubuntu22.04.

Ubuntu22.04----->without ML

Ubuntu22.04+Debian12 docker------>ML/non-ML

Best Regards,
Zhiming

0 Kudos
Reply

2,527 Views
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

We tested on two different Ubuntu 22.04 PCs, both using the Debian 12 Docker image provided by NXP.

However, the compilation still failed.

Do you have any suggestions?"

0 Kudos
Reply

2,491 Views
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

Thanks for your help.

We change use the Azure VM (Cloud vm), the result is pass.

Tags (1)
0 Kudos
Reply

2,555 Views
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

May I compile without ML?
Do you have any advice?

Thanks.

Tags (1)
0 Kudos
Reply